ELES, d.o.o., is the combined transmission and distribution system operator of the Republic of Slovenia. When they set out to build their latest IEC 61850 station bus at a new substation, ELES recognized they would need an advanced Ethernet networking solution capable of sending critical protection traffic securely and reliably between substations. Learn how the utility determined that operational technology software-defined networking (OT SDN) would be the best solution.
Currently loaded videos are 1 through 15 of 670 total videos.